This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP175: Is t(sudat) of FAST MODE 100ns(min)?

Part Number: TMP175
Other Parts Discussed in Thread: TMP75

HI staff.
Check the change history.

The Revison Hostory of the TMP175,TMP75 data sheets (SBOS288M) has the following changes.

• Changed minimum Data setup specification time from 10 ns to 20 ns...............................................................7

I think this change is related to the MIN value of HIGH-SPEED MODE.
The "t(sudat)" of FAST MODE is 100ns (min). Is this value unchanged?

best regards
cafain