Other Parts Discussed in Thread: AWR2243, TDA2, AWR1243
Hello team,
Customer had buy one set of MMWCAS-DSP-EVM. with AWR2243 cascade RF board.
But during the test, customer had sucessful burn the SD card with the correct image( vision sdk radar-3.8 pre-build image).
But during the test, they will fail 9 times at 10 times boot.
Also, i had help customer fix several EVM HW bug.
Question. what's the issue while the board have below log information?
And, is the board do the test before ship it out?
Thanks.
TDA2xx SBL Boot
DPLL Configuration Completed
Clock Domain Configuration Completed
Module Enable Configuration Completed
TI EVM PAD Config Completed
ERROR: HW-Leveling time-out
DDR Config Completed
App Image Download Begins
SD Boot - file open completed successfully
Invalid Magic String in Boot Image
Invalid Magic String in Boot Image
Invalid Magic String in Boot Image
Invalid Magic String in Boot Image
Invalid Magic String in Boot Image
Invalid Magic String in Boot Image
Invalid Magic String in Boot Image
Valid App Image is not Available
Putting MPU CPU1 in Off mode
*****************************************************************
PMCCNTR counts once every 64 clock cycles, multiple by 64 to get actual CPU cycles
SBL Initial Config Cycles - 124327 (10.60 ms)
SOC Init Cycles - 170851 (14.57 ms)
DDR Config Clock Cycles - 131108 (11.18 ms)
App Image Load Cycles - 41816656 (3568.35 ms)
Slave Core Bootup Cycles - 54227 (4.62 ms)
SBL Boot-up Cycles - 42298230 (3609.44 ms)
Time at which SBL started IPU1_0 - 127831 (3901.9 ms)
*****************************************************************
Putting MPU in Retention...
Regards,
Wesley