Hi, so I am working on lab4 obstacle detection and I want to know whether in this lab we are using MIMO configuration and if so which one, BPM or TDM ( I think it's Bpm but im not quite sure ) ?
and Q2 : I want to replace the GUI of Matlab which i use to send chirp configuration file so when I debug the lab4 on code composer it sends automatically the chirp configuration, I asked such a question before and I was shown the example of lab5 but I did not quite know what should I modify in the code and whether it should be in the MSS project or the DSS or elsewhere.
Thanks