Other Parts Discussed in Thread: AWR1243
Hi TI,
During recent testing with ES1.1 AWR2243 MMIC, we ran into BSS CPU fault that resulted in initial calibration failure as well as Host IRQ timeout for Profile config.
I have attached the variable watch data that provides the CPU fault details as well as results of initial calibration.
The calibration results also indicate SYNTH VCO1 calibration failed along with PD and TX power. Is there a possibility that the BSS CPU fault triggered by SYNTH VCO calibration failure like we saw with AWR1243 MMICs? The sensor went through AB swap as it had originally failed for EDMA BIST failure. However, after the AB swap we started seeing this issue with the RF board that has the good MMIC.
The sensors are running with DFP 2.2.1.2 and have factory calibration done with same FW version.
Could you please take a look at the CPU fault and let us know what you find?
Thanks,
Kaushal
gDeviceSpiBootUpComp.unsigned char.1 Byte(s).1 .0x01 - . gDevicePowerUpComp.unsigned char.1 Byte(s).1 .0x01 - . BssCpuFaultReport.rlCpuFault.32 Byte(s).. faultType.unsigned char.1 Byte(s).3 .0x03 - . errorCode.unsigned char.1 Byte(s).0 .0x00 . lineNum.unsigned short int.2 Byte(s).1702 .0x06A6 . faultLR.unsigned int.4 Byte(s).103962 .0x0001961A . faultPrevLR.unsigned int.4 Byte(s).0 .0x00000000 . faultSpsr.unsigned int.4 Byte(s).536871199 .0x2000011F . faultSp.unsigned int.4 Byte(s).134281472 .0x0800F900 . faultAddr.unsigned int.4 Byte(s).0 .0x00000000 . faultErrStatus.unsigned short int.2 Byte(s).65535 .0xFFFF . faultErrSrc.unsigned char.1 Byte(s).255 .0xFF - ÿ. faultAxiErrType.unsigned char.1 Byte(s).255 .0xFF - ÿ. faultAccType.unsigned char.1 Byte(s).255 .0xFF - ÿ. faultRecovType.unsigned char.1 Byte(s).255 .0xFF - ÿ. reserved1.unsigned short int.2 Byte(s).0 .0x0000 . measRing.rfInit..80 Byte(s).. elements[3]..60 Byte(s).. elements[0].RFC_RfInit.20 Byte(s).. un_calibStatus..4 Byte(s).. bitfield..4 Byte(s).. RESERVED_1.unsigned char.1 Bits.0 .0x00 . APLL_tuning.unsigned char.1 Bits.0 .0x00 . SYNTH_VCO1_tuning.unsigned char.1 Bits.0 .0x00 . SYNTH_VCO2_tuning.unsigned char.1 Bits.0 .0x00 . LODIST_calibration.unsigned char.1 Bits.0 .0x00 . RX_ADC_DC_offset_calibration.unsigned char.1 Bits.0 .0x00 . HPF_cutoff_calibration.unsigned char.1 Bits.0 .0x00 . LPF_cutoff_calibration.unsigned char.1 Bits.0 .0x00 . Peak_detector_calibration.unsigned char.1 Bits.0 .0x00 . TX_Power_calibration.unsigned char.1 Bits.0 .0x00 . RX_gain_calibration.unsigned char.1 Bits.0 .0x00 . TX_Phase_calibration.unsigned char.1 Bits.0 .0x00 . RX_IQMM_calibration.unsigned char.1 Bits.0 .0x00 . RESERVED_3.unsigned int.19 Bits.0 .0x00000000 . u32_value.unsigned int.4 Byte(s).0 .0x00000000 . un_calibUpdate..4 Byte(s).. bitfield..4 Byte(s).. RESERVED_1.unsigned char.1 Bits.0 .0x00 . APLL_tuning.unsigned char.1 Bits.0 .0x00 . SYNTH_VCO1_tuning.unsigned char.1 Bits.0 .0x00 . SYNTH_VCO2_tuning.unsigned char.1 Bits.0 .0x00 . LODIST_calibration.unsigned char.1 Bits.0 .0x00 . RX_ADC_DC_offset_calibration.unsigned char.1 Bits.0 .0x00 . HPF_cutoff_calibration.unsigned char.1 Bits.0 .0x00 . LPF_cutoff_calibration.unsigned char.1 Bits.0 .0x00 . Peak_detector_calibration.unsigned char.1 Bits.0 .0x00 . TX_Power_calibration.unsigned char.1 Bits.0 .0x00 . RX_gain_calibration.unsigned char.1 Bits.0 .0x00 . TX_Phase_calibration.unsigned char.1 Bits.0 .0x00 . RX_IQMM_calibration.unsigned char.1 Bits.0 .0x00 . RESERVED_3.unsigned int.19 Bits.0 .0x00000000 . u32_value.unsigned int.4 Byte(s).0 .0x00000000 . temperature.short int.2 Byte(s).0 .0x0000 . reserved0.unsigned short int.2 Byte(s).0 .0x0000 . timeStamp.unsigned int.4 Byte(s).0 .0x00000000 . reserved1.unsigned int.4 Byte(s).0 .0x00000000 . elements[1].RFC_RfInit.20 Byte(s).. un_calibStatus..4 Byte(s).. bitfield..4 Byte(s).. RESERVED_1.unsigned char.1 Bits.0 .0x00 . APLL_tuning.unsigned char.1 Bits.1 .0x01 - . SYNTH_VCO1_tuning.unsigned char.1 Bits.0 .0x00 . SYNTH_VCO2_tuning.unsigned char.1 Bits.0 .0x00 . LODIST_calibration.unsigned char.1 Bits.0 .0x00 . RX_ADC_DC_offset_calibration.unsigned char.1 Bits.1 .0x01 - . HPF_cutoff_calibration.unsigned char.1 Bits.1 .0x01 - . LPF_cutoff_calibration.unsigned char.1 Bits.1 .0x01 - . Peak_detector_calibration.unsigned char.1 Bits.0 .0x00 . TX_Power_calibration.unsigned char.1 Bits.0 .0x00 . RX_gain_calibration.unsigned char.1 Bits.1 .0x01 - . TX_Phase_calibration.unsigned char.1 Bits.0 .0x00 . RX_IQMM_calibration.unsigned char.1 Bits.1 .0x01 - . RESERVED_3.unsigned int.19 Bits.262144 .0x00040000 . u32_value.unsigned int.4 Byte(s).2147488994 .0x800014E2 . un_calibUpdate..4 Byte(s).. bitfield..4 Byte(s).. RESERVED_1.unsigned char.1 Bits.0 .0x00 . APLL_tuning.unsigned char.1 Bits.0 .0x00 . SYNTH_VCO1_tuning.unsigned char.1 Bits.0 .0x00 . SYNTH_VCO2_tuning.unsigned char.1 Bits.0 .0x00 . LODIST_calibration.unsigned char.1 Bits.0 .0x00 . RX_ADC_DC_offset_calibration.unsigned char.1 Bits.1 .0x01 - . HPF_cutoff_calibration.unsigned char.1 Bits.1 .0x01 - . LPF_cutoff_calibration.unsigned char.1 Bits.1 .0x01 - . Peak_detector_calibration.unsigned char.1 Bits.0 .0x00 . TX_Power_calibration.unsigned char.1 Bits.0 .0x00 . RX_gain_calibration.unsigned char.1 Bits.1 .0x01 - . TX_Phase_calibration.unsigned char.1 Bits.0 .0x00 . RX_IQMM_calibration.unsigned char.1 Bits.1 .0x01 - . RESERVED_3.unsigned int.19 Bits.0 .0x00000000 . u32_value.unsigned int.4 Byte(s).5344 .0x000014E0 . temperature.short int.2 Byte(s).27 .0x001B . reserved0.unsigned short int.2 Byte(s).0 .0x0000 . timeStamp.unsigned int.4 Byte(s).0 .0x00000000 . reserved1.unsigned int.4 Byte(s).15 .0x0000000F . elements[2].RFC_RfInit.20 Byte(s).. un_calibStatus..4 Byte(s).. bitfield..4 Byte(s).. RESERVED_1.unsigned char.1 Bits.0 .0x00 . APLL_tuning.unsigned char.1 Bits.0 .0x00 . SYNTH_VCO1_tuning.unsigned char.1 Bits.0 .0x00 . SYNTH_VCO2_tuning.unsigned char.1 Bits.0 .0x00 . LODIST_calibration.unsigned char.1 Bits.0 .0x00 . RX_ADC_DC_offset_calibration.unsigned char.1 Bits.0 .0x00 . HPF_cutoff_calibration.unsigned char.1 Bits.0 .0x00 . LPF_cutoff_calibration.unsigned char.1 Bits.0 .0x00 . Peak_detector_calibration.unsigned char.1 Bits.0 .0x00 . TX_Power_calibration.unsigned char.1 Bits.0 .0x00 . RX_gain_calibration.unsigned char.1 Bits.0 .0x00 . TX_Phase_calibration.unsigned char.1 Bits.0 .0x00 . RX_IQMM_calibration.unsigned char.1 Bits.0 .0x00 . RESERVED_3.unsigned int.19 Bits.0 .0x00000000 . u32_value.unsigned int.4 Byte(s).0 .0x00000000 . un_calibUpdate..4 Byte(s).. bitfield..4 Byte(s).. RESERVED_1.unsigned char.1 Bits.0 .0x00 . APLL_tuning.unsigned char.1 Bits.0 .0x00 . SYNTH_VCO1_tuning.unsigned char.1 Bits.0 .0x00 . SYNTH_VCO2_tuning.unsigned char.1 Bits.0 .0x00 . LODIST_calibration.unsigned char.1 Bits.0 .0x00 . RX_ADC_DC_offset_calibration.unsigned char.1 Bits.0 .0x00 . HPF_cutoff_calibration.unsigned char.1 Bits.0 .0x00 . LPF_cutoff_calibration.unsigned char.1 Bits.0 .0x00 . Peak_detector_calibration.unsigned char.1 Bits.0 .0x00 . TX_Power_calibration.unsigned char.1 Bits.0 .0x00 . RX_gain_calibration.unsigned char.1 Bits.0 .0x00 . TX_Phase_calibration.unsigned char.1 Bits.0 .0x00 . RX_IQMM_calibration.unsigned char.1 Bits.0 .0x00 . RESERVED_3.unsigned int.19 Bits.0 .0x00000000 . u32_value.unsigned int.4 Byte(s).0 .0x00000000 . temperature.short int.2 Byte(s).0 .0x0000 . reserved0.unsigned short int.2 Byte(s).0 .0x0000 . timeStamp.unsigned int.4 Byte(s).0 .0x00000000 . reserved1.unsigned int.4 Byte(s).0 .0x00000000 . ctrl..20 Byte(s).. spCount[3]..12 Byte(s).. spCount[0].unsigned int.4 Byte(s).0 .0x00000000 . spCount[1].unsigned int.4 Byte(s).1 .0x00000001 . spCount[2].unsigned int.4 Byte(s).0 .0x00000000 . filledElements.unsigned int.4 Byte(s).1 .0x00000001 . currIdx.unsigned int.4 Byte(s).1 .0x00000001 . ar12Cfg.mmicInitCalibStatus..1 Byte(s).1 .INIT_CALIB_FAIL . ar12Cfg.factoryCalibDone.unsigned char.1 Byte(s).1 .0x01 - .