This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR6843AOPEVM: Height measurement changes when moving away from the sensor - people counting/fall detection

Part Number: IWR6843AOPEVM


Hello, while testing with the people counting binary and demo, I noticed that the height of the object's centroid reduces when I move further away from the sensor, and increases when I move closer.

Is there a way to compensate for this change of height when the object moves along the x and y-axis? 

Thank you!

  • Hi, 

    Can you please provide more details

    - sensor mounting height

    - at what distance do you see the issue 

    - what is the magnitude of error that you observe? 

    Regards, 

    Sudharshan K N 

  • Hello,

    The sensor is mounter at 1.82m, with an elevation of 10 degrees.

    The issue occurs at every distance.

    When I stand 30cm away from the sensor, my height is 150cm, when I move to 130cm away, my height is 130cm and when I'm at 280cm away, by height was only 90cm. 

    I checked the height using both the centroid height and the height of the highest point in the target.

    When we move away, we can see something like a linear drop from the height values. 

    This problem will cause errors in some fall detection cases.

  • Hi, 

    Can you please confirm if the issue occurs even when the elevation is 0deg? Meaning no tilt to the sensor? If the issue happens only when the sensor is tilted may be we need to check the configuration to see if this is already included. 

    Regards, 

    Sudharshan K N

  • Hi, it still occurs at 0 deg elevation.

    Cheers,

    Danh

  • Hi, 

    Can you please provide us more details as how the height is determined? is the senor mounted on the wall or ceiling? Also if you are using any reference lab from TiREX please provide us the lab name that your code is based off. 

    Regards, 

    Sudharshan K N 

  • Hi,

    The height is determined by using the point with the highest Z coordinate in the target. The sensor is wall mounted. The code is based on the people counting lab.

    Thanks

  • Hi, 

    We will get back to you with this by next week. In the meanwhile if you have additional data files please share it with us. 

    - Chirp configuration used 

    - Setup details 

    - Data collected to verify the height

    Regards, 

    Sudharshan K N 

  • Hi, I'll be waiting for your reply. Here's the chirp config I'm using:

    """

    sensorStop
    flushCfg
    dfeDataOutputMode 1
    channelCfg 15 7 0
    adcCfg 2 1
    adcbufCfg -1 0 1 1 1
    lowPower 0 0
    profileCfg 0 60.75 30.00 25.00 59.10 394758 0 54.71 1 96 2950.00 2 1 36
    chirpCfg 0 0 0 0 0 0 0 1
    chirpCfg 1 1 0 0 0 0 0 2
    chirpCfg 2 2 0 0 0 0 0 4
    frameCfg 0 2 96 0 55.00 1 0
    dynamicRACfarCfg -1 4 4 2 2 8 12 4 8 5.00 8.00 0.40 1 1
    staticRACfarCfg -1 6 2 2 2 8 8 6 4 8.00 15.00 0.30 0 0
    dynamicRangeAngleCfg -1 0.75 0.0010 1 0
    dynamic2DAngleCfg -1 1.5 0.0300 1 0 1 0.30 0.85 8.00
    staticRangeAngleCfg -1 0 8 8
    antGeometry0 -1 -1 0 0 -3 -3 -2 -2 -1 -1 0 0
    antGeometry1 -1 0 -1 0 -3 -2 -3 -2 -3 -2 -3 -2
    antPhaseRot 1 -1 1 -1 1 -1 1 -1 1 -1 1 -1
    fovCfg -1 70.0 20.0
    compRangeBiasAndRxChanPhase 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
    staticBoundaryBox -1.3 1.5 0.85 4 0 2.67
    boundaryBox -1.3 1.5 0.7 4 0 2.67
    sensorPosition 1.82 0 10
    gatingParam 3 2 2 2 4
    stateParam 4 4 8 100 5 6000
    allocationParam 60 200 0.1 35 0.5 20
    maxAcceleration 0.1 0.1 0.1
    trackingCfg 1 2 600 4 46 96 55
    presenceBoundaryBox -1.3 1.5 0.7 4 0 2.67
    sensorStart

    """

    The setup looks like this:

    Where the sensor is 1.82m high with an elevation of 10 degrees. When a target moves further away from the sensor, doing the same action (in my case shaking the head so point clouds are generated there), we can see that the height of the object drops linearly when they are further away, and increases when they move closer. Here, the subject is 1.55m tall in real life, and how it's shown when he walked away from the sensor, doing the same action

    You can see the slope going down.

    Thanks.

  • The plot axis are y- height and x - distance from sensor.

  • Hello, do you have any updates regarding this height problem?

  • Hi, 

    Can you please try to do the tests with a strong object like corner reflector and verify the results? 

    Regards, 

    Sudharshan K N