Part Number: OPT3001
Other Parts Discussed in Thread: OPT3007
I need help in choosing a sensor that just provides a digital logic signal in terms of 0 and 1. For example, if there is light then sensor output should be 1, and when there is no light then 0. I want to make my product as simple as possible in terms of programming as well as circuit designing. I have to integrate this sensor in a keypad where it will turn ON/OFF backlight according to the day and night. I am already using I2C based sensor but it requires some resistors and capacitors which I want to avoid and also it needs a little complex program to monitor than a simple logic program. I hope it will clear my question. Let me know if I missed something. Thanks