Hi,
It is mentioned in the following thread that the elevation FoV is 44 degrees while the elevation angle resolution is 58 degrees.
I am trying to make sense of these figures from a practical perspective and things don't make sense. According to my understanding, based on the elevation FoV angle of 44 degrees, no two objects (at the same range and the same velocity) separated by more than 44 degrees in the elevation dimension can be detected by the radar at the same time. Therefore, even if two objects are separated by 58 degrees in the elevation direction and one of those objects is within the elevation field of view, the other one will not be detectable anyways. So the elevation resolution seems to be a redundant measure in this example.
What this tells me from a practical perspective is, if two objects (at the same range and velocity) are within 44 degrees or less with respect to each other along the elevation direction, they cannot be differentiated at all. In other words, trying to differentiate two such objects within the elevation FoV using IWR6843ISK device is not possible.
Can you please confirm and if my understanding is not correct, can you please elaborate using real world examples of how this would work?
Thank you for your help.
Regards,
Cagri