This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR6843AOP: How to detect small box

Part Number: AWR6843AOP


Hi Team,

Our customer is using AWR6843AOP and needs help on detecting small box. According to the customer,

I need to detect a 20cm x 20cm x 20cm box
in "Area Scanner" lab
at "Tracked Objects"
by AWR6843AOP

in test a 20cm x 20cm x 20cm box
only detected in "Dynamic Point Cloud"
sometimes in shortly tracked

how can i detect a mini box by AWR6843AOP and use "Tracked Objects" function?

can you give me a list of be changed setting value and a example value?

Regards,

Danilo

  • Danilo:

    I would suggest starting with the OOB demo. Then I would play around with the CLI commands frameConfig, profileConfig, chirpConfig, etc. To see how well you can detect the box. With regards to area scanner or the object tracking these are more advanced demos which build off of the OOB demo, so starting with the OOB is the best place to start. If you are already familiar with the OOB then I would dig into the collateral provided in the Area Scanner demo.

    CLI Command Descriptions - SDK Section 3.4

    <MMWAVE SDK INSTALL PATH>\mmwave_sdk_03_05_00_04\docs\mmwave_sdk_user_guide.pdf

    Best regards,

    Connor Desmond