Other Parts Discussed in Thread: IWR6843ISK, ,
Hello,
I want to use BeamForming in order to focus radar detection area and improve its SNR, no need for distance improvement.
I am currently working with IWR6843ISK eval board, SDK 3.05.00.04, and I succeeded using 2TX and 3TX Beamforming. I got as predicted a restricted emission cone of +/-11.25° in azimuth for the central lobe. I used the manual “Enable TX beamforming” in the Industrial Toolbox 4.7.0 as reference.
I want to compare my result to IWR6843AOPEVM board ones. It seems that BeamForming and BeamSteering are achievable with the AOP version of the chip, and the MM BeamSteering Lab of Automotive Toolbox 3.3.0 seem to give an example of that.
Unfortunately, I cannot find these pieces of information, could you please answer these questions:
- Can you confirm that IWR6843AOP antennas are compatible with BeamForming and BeamSteering and that SDK 3.05.00.04 can let me implement it?
- What detection cone could we obtain through combining 2TX Azimuth? And 3TX at the same time?
- Is the calculation law described in “Enable TX BeamForming” document modifiable to use with the AOP version, did someone already did this? If you have an example, Python or Matlab script for example, I would really appreciate this.
- Do you have specific recommendations or warnings into porting my current ISK app (derived from OOB Demo) into an AOP compatible one?
Thank you very much for your help, best regards, Fabien.
mmWave SDK 3.05.00.04, TI RTOS bios 6.73.01.01
eval kit: IWR6843ISK ES2 rev.d
compiler ti cgt 16.9.6.LTS, CCS 10.3.0.00007