Would need to know what TMP124 consumption in active mode, and the SPI bus turn on and off
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Would need to know what TMP124 consumption in active mode, and the SPI bus turn on and off
HI Eduardo,
We don't have any data to share with you currently. I will have to connect this in the lab and test for you.
The current consumption is going to depend heavily on two things:
1.) How often are you reading from the TMP124?
2.) What is the SPI clock frequency?
So I make sure I take data that is meaningful to you, please inform me of the conditions above that you are interested in. My equipment is setup to run at +3.3V so unless you object that is the supply voltage I plan to use for the test.
Regards,
Collin Wells
The TMP124 I read every 1 sec approx.
SPI frequency is 250 KHz or 400KHz.
The power is 3 batteries of Li and 3.3 V regulator (REG1117A-3.3)
This will need to determine an average consumption when this active and reading and when in standby, no shutdown.
To calculate the measurement time maximums of TMP124, without taking regulatory considering battery power.
Thank you very much
EduardoBan
Hello Eduardo,
I was able to perform the testing on the TMP124 today. Please note that these tests were only performed on one unit and the results across all units will vary, but this should give you a good idea of what to expect.
I setup the SPI sequence to be as continuous as possible (little delay between /CS periods). Although this is not a realistic form of operation, I needed to do it to be sure that I wasn't reading an averaged current with the part in standby-mode part of the time and in SPI-operation part of the time.
Measured Currents:
Standby - 53uA
250kHz SPI - 75uA
400kHz SPI - 87uA
Please find an image of the 250kHz reads below:
400kHz reads:
Best Regards,
Collin Wells
Precision Analog
Hello,
I forgot to add that I was using an MSP430FG4618 to generate these signals.
Regards,
Collin Wells
Precision Analog
Thank you very much for the reply, I am using a system of measurement for battery-powered and needed to compare with other devices from Analog Device.
thank you very much
Eduardo Ban