Hello
I have a question about range detection of two objects which are in the same bin
For example
1. Bin 10 has an object with a size of 100 and a phase of 30 degree
2.. Objects with size 100 but phase (180+30) degree added to bin 10
(When two objects fall by a quarter of their wavelength.)
In this case, I think that the Range FFT result for bin 10 will be zero.
(Because Bin 10 has two objects which have same magnitude but phase diff 180)
Although there are two objects in Bin 10, the measurement result is that bin 10 has no objects,
Becasue In this case bin 10 is not peak but zero amplitude . I think Doppler FFT is impossible isn't it?
I want to know how to avoid this situation