This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3101: TOF Sensor Query on Maximum and Minimum Distance of Coverage

Part Number: OPT3101

HI 

We need to use the OPT3101 ToF Sensor for calculating the distance to the object in two different ranges on the same product.

Our requirements are

1.10m

2. 40m

a) How to adjust the range of the sensor for these two application?

b)What is the range offered by the OPT3101EVM evaluation module?

c) What is the resolution(Accuracy) of the sensor?