Other Parts Discussed in Thread: AWR1642
Hi, I am doing some tests with the OOB demo lab for the awr1642, I am using the mmwave_industrial_toolbox_4_7_0 (latest) and the release note say that the SDK 2.0.0.4 is required, ok, but in the ti\mmwave_sdk_03_05_00_04\packages\ti\demo\xwr16xx\mmw directory there are also source files for the awr1642 OOB demo and these files are not the same as the ti\mmwave_sdk_02_00_00_04\packages\ti\demo\xwr16xx\mmw , so it seems like there is an updated version of the OOB lab for the awr1642 inside the SDK 3.5.0.4 but not available in TIREX, why?
and, how could I use the files in the ti\mmwave_sdk_03_05_00_04\packages\ti\demo\xwr16xx\mmw directory to create an OOB demo project for the awr1642 but compatible with the sdk 3.5.0.4 version, is this possible?
thanks