This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: Setting values do not match between mmWaveStudio GUI and mmWaveStudio CLI

Part Number: AWR1843


I have a question about the setting values of mmWaveStuido CLI Tool.

Question 1
The decimal point in ProfileCfg is truncated.

JSON file generated by mmWaveStudio GUI
 "adcStartTimeConst_usec": 5.5,
 "rampEndTime_usec": 40.630001068115234,
 "freqSlopeConst_MHz_usec": 88.061996459960938,

Log when running mmWaveStuido CLI Tool
 profileCfg  0 77.00 10 5 40 0 0 88.06 0 256 7502 0 0 30


Question 2
It seems that the setting value of DataConfig cannot be checked in the CLI Tool log, is there any way to check it?

*It is the following part of mmWaveStudio GUI

  • Hello User,

    Thankyou for reaching out on TI E2E forums. 

    Our expert will get back to your concern by tomorrow or early next week. 

    Thankyou for your patience. 

    Regards,

    Ishita

  • 1.  Looks like these are converted to integer instead of float value which is causing converted cfg file to have truncated values.

    Fix: 

    gui\mmw_cli_tool\serial_comm\mmwave_json_parser.c  :  int writeCliCfg() function

    Under

    for (idx = 0; idx < gMmwSensCfg.rfCfg.profileCfgCnt; idx++)

    {

    .....

    .....

    /* change sprintf code snippet to save final converted values in float */

    sprintf(cliStr, "%s %d %.2f %.2f %.2f %.2f %d %d %.2f %d %d %d %d %d %d %c", defaultCliCmd[PROFLIE_CFG], profCfgPtr->profileId, \
    (float)START_FREQ_GHZ_CONVERSION(profCfgPtr->startFreqConst), (float)profCfgPtr->idleTimeConst / 100, \
    (float)profCfgPtr->adcStartTimeConst / 100, (float)profCfgPtr->rampEndTime / 100, profCfgPtr->txOutPowerBackoffCode, \
    profCfgPtr->txPhaseShifter, (float)FREQ_SLOP_MHz_CONVERSION(profCfgPtr->freqSlopeConst), profCfgPtr->txStartTime, \
    profCfgPtr->numAdcSamples, profCfgPtr->digOutSampleRate, profCfgPtr->hpfCornerFreq1, \
    profCfgPtr->hpfCornerFreq2, profCfgPtr->rxGain, teminatStr);

    Rebuild the Studio CLI tool

    2. Studio CLI doesn't provide much flexibility to control the datapath (i.e. those LVDS lane, data length, speed etc.) You need to change that in the device application available under src directory.

  • Thank you for your answer.

    1. I have solved the problem with the following modification.

    C:\ti\mmwave_platform_1_2_1\tools\studio_cli\gui\mmw_cli_tool\serial_comm\mmwave_json_parser.c

    		sprintf(cliStr, "%s %d %.2f %.2f %.2f %.2f %d %d %f %d %d %d %d %d %d %c", defaultCliCmd[PROFLIE_CFG], profCfgPtr->profileId, \
    			(float)START_FREQ_GHZ_CONVERSION(profCfgPtr->startFreqConst), (float)profCfgPtr->idleTimeConst / 100, \
    			(float)profCfgPtr->adcStartTimeConst / 100, (float)profCfgPtr->rampEndTime / 100, profCfgPtr->txOutPowerBackoffCode, \

    2. I understand.