Other Parts Discussed in Thread: MMWCAS-RF-EVM, AWR2243
Dear TI team,
I am using the board MMWCAS-DSP-EVM (with the MMWCAS-RF-EVM) since several months ago without any problem.
I am using the HW in 2 ways :
the way N°1: mmWave version : mmwave_studio_03_00_00_14 Firmware version: sdimage_3_7_1.img.xz. the S4 switch is setup to 110000
the way N°2: SDK: PROCESSOR_SDK_VISION_03_08_00_00 the SDK code is adapted to AWR2243 and is running correctly since 4 months ago.
I think it is not a SW or FW issue. I think that the SD card reader is down and is not able to boot the SD card again.
please find attached the serial log obtained when I try to run the evaluation module.