Other Parts Discussed in Thread: SYSCONFIG
Hello,
as I need one more GPIO I redefined P4 (SYNC_OUT) to GPIO28 via sysconfig.
Includes were added to mss_main.c
#include "pin_mux_config.h"
#include <ti/drivers/pinmux/pinmux.h>
in routine SRR_MSS_mssProcessDataPathTask I added
Pinmux_Set_OverrideCtrl(SOC_XWR18XX_PINP4_PADBB, PINMUX_OUTEN_RETAIN_HW_CTRL, PINMUX_INPEN_RETAIN_HW_CTRL);
Pinmux_Set_FuncSel(SOC_XWR18XX_PINP4_PADBB,SOC_XWR18XX_PINP4_PADBB_GPIO_28);
pin_mux_config.h and the sysconfig file were added to the project directory.
During compilation this failed:
"../mss_main.c", line 741: error #20: identifier "SOC_XWR18XX_PINP4_PADBB" is undefined
"../mss_main.c", line 742: error #20: identifier "SOC_XWR18XX_PINP4_PADBB_GPIO_28" is undefined
Could you please tell me what went wrong here?
Thanks a lot!
Christoph