This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP61: suggestion on probe to use

Part Number: TMP61

Hello Guys,

Good day.

Our customers application is to 'dangle' a probe in two different types of gas flows and they are looking for sensors which have a range 0 to 100 deg C and is considering to use TMP61.

What physical probe can they use with TMP61 and does the response time change depending on the physical probe? Also, how do they attach physical probes (to be dangled into the air flow for instance)?

They are essentially looking for a probe like this but if you have better suggestions, that is very much welcomed: www.omega.com/.../TH-10-44006-1-8-4-40

Thank and regards,

Art