This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: Sensor identifies water from shower as a target

Part Number: IWR6843AOPEVM

Hello,

I tried running the People detection/fall detection lab in my bathroom, with the shower on.

And the sensor identifies the water from the shower hose as a target.

What can I do to stop the sensor from identifying water as a target?

I am using the people counting Binary and below is my config:

sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 7 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
lowPower 0 0
profileCfg 0 60.75 30.00 25.00 59.10 394758 0 54.71 1   96 2950.00 2 1 36 
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
chirpCfg 2 2 0 0 0 0 0 4
frameCfg 0 2  96  0 55.00 1 0
dynamicRACfarCfg -1 4 4 2 2 8 12 4 8 5.00 8.00 0.40 1 1
staticRACfarCfg -1 6 2 2 2 8 8 6 4 8.00 15.00 0.30 0 0
dynamicRangeAngleCfg -1 0.75 0.0010 1 0
dynamic2DAngleCfg -1 1.5 0.0300 1 0 1 0.30 0.85 8.00
staticRangeAngleCfg -1 0 8 8
antGeometry0 -1 -1 0 0 -3 -3 -2 -2 -1 -1 0 0
antGeometry1 -1 0 -1 0 -3 -2 -3 -2 -3 -2 -3 -2
antPhaseRot 1 -1 1 -1 1 -1 1 -1 1 -1 1 -1
fovCfg -1 60.0 50.0
compRangeBiasAndRxChanPhase 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 
staticBoundaryBox -1.5 2.0 0.8 4.0 0.0 2.9 
boundaryBox -1.5 2.0 0.8 4.0 0.0 2.9 
sensorPosition 1.92 0 15 
gatingParam 3 2 2 2 4
stateParam 4 4 8 100 5 6000
allocationParam 50 185 0.1 35 0.5 20
maxAcceleration 0.3 0.3 0.3
trackingCfg 1 2 600 4 46 96 55 
presenceBoundaryBox -1.5 2.0 0.8 4.0 0.0 2.9 
sensorStart

Thank you!