Other Parts Discussed in Thread: IWR1443, DCA1000EVM
I have been collecting data with the iwr1443 radar and had some questions regarding the dca1000EVM board used in conjunction with it. My main question is that I see in newer SDK versions there is support for logging the adc samples using the mmwave demos. However in the newest version, I see for the IWR1443 (mmwave_sdk_02_00_00_04) I do not see support for this functionality. My question is do you have a build that can support dca1000EVM logging in conjunction with the demo for the IWR1443 radar? If not do you have a uart library to enabling logging dca logging? My main goal is to remove dependency of mmwave studio for field logging.