This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK-ODS: More information on Configuration files

Genius 9880 points
Part Number: IWR6843ISK-ODS


Hi,

Good day.

Customer is looking for more information about of the following configuration files. See inquiry below.

"

I have some questions concerning the chirp configuration. Can I write assertions and if possible you tell me if their are true or not ?

I would like more information on configuration files. What each field of a command stands for maybe there is already a document for that ? I just can't find it.

dynamicRACfarCfg
staticRACfarCfg
dynamicRangeAngleCfg
dynamic2DAngleCfg
staticRangeAngleCfg
antGeometry
antPhaseRot
fovCfg
compRangeBiasAndRxChanPhase
staticBoundaryBox
boundaryBox
sensorPosition
gatingParam
stateParam
allocationParam
maxAcceleration
trackingCfg

"

According to customer they got in the  in the .cfg file for the 3D people people counting demo in the indrustrial toolboox. \ti\mmwave_industrial_toolbox_4_7_0\labs\people_counting\68xx_3D_people_counting\chirp_configs.

ISK_6m_default (1).cfg

Thank you in advance.

Regards,
Maynard