Hello Experts,
I am designing a ground penetrating radar system that I am going to hold at about 1 meter over the ground distance. I only need to see 0.5 meter depths with 0.05 meter range resolution. Would anyone happen to know if the generated signal from AWR1843AOPEVM has enough power to penetrate 0.5 meters into the ground? The second object inside the ground is going to be metallic and the ground is just dry soil so I assume that relative permittivity is going to be differing enough. If not is there any other sensor that could give me such penetration power?
Any help or an advice would be highly appreciated.
Thank you