This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: Maximum Range

Part Number: IWR1642BOOST

Hi E2E,

Good day.

Our customer was able to achieve an 80m range using the short range radar lab in the toolbox. However, this range is achieved only for an object with an approximate RCS of 10 sq.m., a bicycle with a lower RCS is detected only up to 20m. What do they need to change in order to extend the detection of bicycles up to 40m? Is changing the CFAR threshold work? If yes, how can they change it?


Regards,
Carlo

  • Hi Carlo

    Lowering CFAR threshold might be helpful but only to a certain extent.

    Otherwise one will want to adjust chirp parameters to better enable detection of a bicycle at long distances. For more information here please see the sensing estimator.

    Regards,

    AG

  • Hello AG,

    Our customer has tried obtaining a configuration from the sensing estimator and tested it, but it did not give the expected results. Here is the configuration file they've used.

    srr_config_cyc_66.56.h

    The 120m configuration included in the demo files seems to detect bicycles up to 50m with a change in CFAR threshold to 12dB. But the problem now is the GUI is lagging drastically and causing troubles for proper visualization. Is there anything that you can suggest to improve performance? Thanking you in advance.

    Regards,
    Carlo

  • Hi Carlo

    I've asked a team member for further support.

    Regards,

    AG

  • Hi,

    The gui performance is related to matlab performance running on PC.

    It is possible to only display alternate frames. In this way the matlab processing will be reduced

    thank you

    Cesar

  • Hello Cesar,

    Here is the response I received from our customer:

    I don't understand the alternate frame displaying concept. Is the given source code already implementing this concept or do I need to make the changes? On the other hand, it would be nice if you can mention any suggestions to improve the performance of Matlab like changing version, reducing payload size, or changing read interval. Please advise, thank you.

    Regards,
    Carlo

  • Hi,

    Alternate frame displaying means that the point cloud is displayed only for one out of two frames.The gui code would have to be modified. This is probably related to what the customer mentions by "changing read interval"

    Regarding improving the performance of matlab we have noticed that with older versions of matlab (2015 or before) the gui works better.

    Thank you

    cesar

  • Hello Cesar,

    According to our customer, the GUI seems to work better with the older version of Matlab. But when they record the data received it is only recorded for a short duration. Is there any method to increase this record duration to 5 mins? Also, do we have some references to change the GUI code to display all frames?

    Regards,
    Carlo

  • Hi,

    The customer can try to increase the value of the "recordingHandle.size"

    gui\read_serial_port_and_plot_object_location.m

    if recordingHandle.enable == 1
        recordingHandle.size = 2^28;
        recordingHandle.indx = 1;
        recordingHandle.array = zeros(recordingHandle.size,1,'uint8');
    end

    By default the GUI code displays all frames.

    thank you
    Cesar

  • Hello Cesar,

    Thank you for sharing the code, according to our customer it works now. However, the GUI seems not to displays all the frames by defaults as for every alternate frame number they see an error frame missed in the Matlab console. Please see the attached file.

    >> read_serial_port_and_plot_object_location
    Error using read_serial_port_and_plot_object_location (line 108)
    Not enough input arguments.
     
    >> srr_ti_design_visualization
    Starting UI for mmWave Demo ....
    Sending configuration to XWR1xxx  ...
    advFrameCfg
    Done
    sensorStart
    Done
    Serial port(s) already open. Re-initializing...
    Warning: checkbox control requires a scalar Value
    Control will not be rendered until all of its parameter values are valid 
    > In read_serial_port_and_plot_object_location (line 369)
      In srr_ti_design_visualization (line 101) 
    Warning: checkbox control requires a scalar Value
    Control will not be rendered until all of its parameter values are valid 
    > In read_serial_port_and_plot_object_location (line 369)
      In srr_ti_design_visualization (line 101) 
    Error: Packets lost: 1, current frame num = 19 
    Error: Packets lost: 1, current frame num = 21 
    RangeM
       56.8672
    
    SpeedM
      -16.1095
    
    Range
       56.8594
    
    Speed
      -16.1094
    
    TTC
        3.5234
    
    Colour
         1
    
    Error: Packets lost: 1, current frame num = 23 
    Warning: checkbox control requires a scalar Value
    Control will not be rendered until all of its parameter values are valid 
    > In read_serial_port_and_plot_object_location (line 369)
      In srr_ti_design_visualization (line 101) 
    RangeM
        6.9945   56.3850
    
    SpeedM
      -16.1599  -16.0956
    
    Range
        6.9922   56.3828
    
    Speed
      -16.1563  -16.0938
    
    TTC
        0.4297    3.5000
    
    Colour
         1     1
    
    Error: Packets lost: 1, current frame num = 25 
    RangeM
        6.5037
    
    SpeedM
      -16.1362
    
    Range
        6.5000
    
    Speed
      -16.1328
    
    TTC
        0.3984
    
    Colour
         1
    
    Error: Packets lost: 1, current frame num = 27 
    Error: Packets lost: 1, current frame num = 29 
    Error: Packets lost: 1, current frame num = 31 
    Error: Packets lost: 1, current frame num = 33 
    Error: Packets lost: 1, current frame num = 35 
    Error: Packets lost: 1, current frame num = 37 
    Error: Packets lost: 1, current frame num = 39 
    Error: Packets lost: 1, current frame num = 41 
    Error: Packets lost: 1, current frame num = 43 
    RangeM
       56.8718
    
    SpeedM
      -16.1536
    
    Range
       56.8672
    
    Speed
      -16.1484
    
    TTC
        3.5156
    
    Colour
         1
    
    Error: Packets lost: 1, current frame num = 45 
    RangeM
       56.3842
    
    SpeedM
      -16.1499
    
    Range
       56.3828
    
    Speed
      -16.1484
    
    TTC
        3.4844
    
    Colour
         1
    
    Error: Packets lost: 1, current frame num = 47 
    RangeM
        8.0561
    
    SpeedM
      -16.1541
    
    Range
        8.0547
    
    Speed
      -16.1484
    
    TTC
        0.4922
    
    Colour
         1
    
    Error: Packets lost: 1, current frame num = 49 
    RangeM
        7.5723
    
    SpeedM
      -16.1518
    
    Range
        7.5703
    
    Speed
      -16.1484
    
    TTC
        0.4688
    
    Colour
         1
    
    Error: Packets lost: 1, current frame num = 51 
    Error: Packets lost: 1, current frame num = 53 
    Error: Packets lost: 1, current frame num = 55 
    RangeM
        9.3638
    
    SpeedM
       -0.0037
    
    Range
        9.3594
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 57 
    RangeM
        9.3638
    
    SpeedM
       -0.0037
    
    Range
        9.3594
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 59 
    RangeM
        9.3569
    
    SpeedM
       -0.0019
    
    Range
        9.3516
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 61 
    RangeM
        9.3579
    
    SpeedM
         0
    
    Range
        9.3516
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 63 
    RangeM
        9.3511
    
    SpeedM
        0.0019
    
    Range
        9.3438
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 65 
    RangeM
        9.3530
    
    SpeedM
        0.0048
    
    Range
        9.3516
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 67 
    RangeM
        9.3472
    
    SpeedM
      8.4918e-05
    
    Range
        9.3438
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 69 
    RangeM
        9.3472
    
    SpeedM
        0.0011
    
    Range
        9.3438
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 71 
    RangeM
        9.3414
    
    SpeedM
        0.0032
    
    Range
        9.3359
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 73 
    RangeM
        7.5072    9.3434
    
    SpeedM
      -16.1762    0.0063
    
    Range
        7.5000    9.3359
    
    Speed
      -16.1719         0
    
    TTC
        0.4609 -100.0000
    
    Colour
         1     2
    
    Error: Packets lost: 1, current frame num = 75 
    RangeM
        7.0208    9.3377
    
    SpeedM
      -16.1706    0.0018
    
    Range
        7.0156    9.3359
    
    Speed
      -16.1641         0
    
    TTC
        0.4297 -100.0000
    
    Colour
         1     2
    
    Error: Packets lost: 1, current frame num = 77 
    RangeM
        9.3387
    
    SpeedM
        0.0030
    
    Range
        9.3359
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 79 
    RangeM
        9.3320
    
    SpeedM
        0.0031
    
    Range
        9.3281
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 81 
    RangeM
        9.3320
    
    SpeedM
        0.0021
    
    Range
        9.3281
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 83 
    RangeM
        9.3299
    
    SpeedM
        0.0065
    
    Range
        9.3281
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 85 
    RangeM
        9.3289   45.3743
    
    SpeedM
        0.0034  -16.0940
    
    Range
        9.3281   45.3672
    
    Speed
             0  -16.0938
    
    TTC
     -100.0000    2.8125
    
    Colour
         2     1
    
    Error: Packets lost: 1, current frame num = 87 
    RangeM
       44.8861    9.3279
    
    SpeedM
      -16.0911    0.0003
    
    Range
       44.8828    9.3203
    
    Speed
      -16.0859         0
    
    TTC
        2.7891 -100.0000
    
    Colour
         1     2
    
    Error: Packets lost: 1, current frame num = 89 
    RangeM
        9.3249
    
    SpeedM
        0.0040
    
    Range
        9.3203
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 91 
    RangeM
        9.3220   44.2744
    
    SpeedM
             0  -16.1123
    
    Range
        9.3203   44.2734
    
    Speed
             0  -16.1094
    
    TTC
     -100.0000    2.7422
    
    Colour
         2     1
    
    Error: Packets lost: 1, current frame num = 93 
    RangeM
        9.3231   43.7874
    
    SpeedM
       -0.0024  -16.1140
    
    Range
        9.3203   43.7813
    
    Speed
             0  -16.1094
    
    TTC
     -100.0000    2.7109
    
    Colour
         2     1
    
    Error: Packets lost: 1, current frame num = 95 
    RangeM
        9.3231
    
    SpeedM
       -0.0024
    
    Range
        9.3203
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 97 
    RangeM
        9.3669
    
    SpeedM
       -0.0019
    
    Range
        9.3594
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 99 
    RangeM
        9.3636   55.9333
    
    SpeedM
        0.0017  -16.1431
    
    Range
        9.3594   55.9297
    
    Speed
             0  -16.1406
    
    TTC
     -100.0000    3.4609
    
    Colour
         2     1
    
    Error: Packets lost: 1, current frame num = 101 
    RangeM
        9.3636   55.4471
    
    SpeedM
       -0.0044  -16.1414
    
    Range
        9.3594   55.4453
    
    Speed
             0  -16.1406
    
    TTC
     -100.0000    3.4297
    
    Colour
         2     1
    
    Error: Packets lost: 1, current frame num = 103 
    RangeM
        9.3596
    
    SpeedM
     -2.0868e-04
    
    Range
        9.3594
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 105 
    RangeM
        9.3588
    
    SpeedM
      5.2214e-05
    
    Range
        9.3516
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 107 
    RangeM
        9.3580
    
    SpeedM
      3.1328e-04
    
    Range
        9.3516
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 109 
    RangeM
        9.3666
    
    SpeedM
       -0.0054
    
    Range
        9.3594
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 111 
    RangeM
        9.3728
    
    SpeedM
       -0.0049
    
    Range
        9.3672
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 113 
    RangeM
        9.3697
    
    SpeedM
       -0.0053
    
    Range
        9.3672
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 115 
    RangeM
        9.3689
    
    SpeedM
       -0.0051
    
    Range
        9.3672
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 117 
    RangeM
        9.3767
    
    SpeedM
       -0.0051
    
    Range
        9.3750
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 119 
    RangeM
        9.3759
    
    SpeedM
       -0.0049
    
    Range
        9.3750
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 121 
    RangeM
        9.4049
    
    SpeedM
        0.0031
    
    Range
        9.3984
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 123 
    RangeM
        9.3902
    
    SpeedM
         0
    
    Range
        9.3828
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 125 
    RangeM
        9.4222   56.4024
    
    SpeedM
        0.0009  -16.1408
    
    Range
        9.4219   56.3984
    
    Speed
             0  -16.1406
    
    TTC
     -100.0000    3.4922
    
    Colour
         2     1
    
    Error: Packets lost: 1, current frame num = 127 
    RangeM
        9.5162   55.9133
    
    SpeedM
             0  -16.1376
    
    Range
        9.5156   55.9063
    
    Speed
             0  -16.1328
    
    TTC
     -100.0000    3.4609
    
    Colour
         2     1
    
    Error: Packets lost: 1, current frame num = 129 
    RangeM
        9.4998
    
    SpeedM
         0
    
    Range
        9.4922
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 131 
    RangeM
        9.4861   55.3101
    
    SpeedM
        0.0018  -16.1447
    
    Range
        9.4844   55.3047
    
    Speed
             0  -16.1406
    
    TTC
     -100.0000    3.4219
    
    Colour
         2     1
    
    Error: Packets lost: 1, current frame num = 133 
    RangeM
        9.4733   54.8272
    
    SpeedM
       -0.0003  -16.1433
    
    Range
        9.4688   54.8203
    
    Speed
             0  -16.1406
    
    TTC
     -100.0000    3.3906
    
    Colour
         2     1
    
    Error: Packets lost: 1, current frame num = 135 
    RangeM
        9.4665
    
    SpeedM
        0.0016
    
    Range
        9.4609
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 137 
    RangeM
        9.4587
    
    SpeedM
        0.0016
    
    Range
        9.4531
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 139 
    RangeM
        9.4596
    
    SpeedM
        0.0017
    
    Range
        9.4531
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 141 
    RangeM
        9.4519
    
    SpeedM
      7.3020e-04
    
    Range
        9.4453
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 143 
    RangeM
        9.4509
    
    SpeedM
     -2.6494e-04
    
    Range
        9.4453
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 145 
    RangeM
        9.4500
    
    SpeedM
        0.0047
    
    Range
        9.4453
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 147 
    RangeM
        9.4491   56.3516
    
    SpeedM
        0.0028  -16.1461
    
    Range
        9.4453   56.3516
    
    Speed
             0  -16.1406
    
    TTC
     -100.0000    3.4844
    
    Colour
         2     1
    
    Error: Packets lost: 1, current frame num = 149 
    RangeM
        9.4473   55.8759   59.2517
    
    SpeedM
             0  -16.1110   -0.0020
    
    Range
        9.4453   55.8750   59.2500
    
    Speed
             0  -16.1094         0
    
    TTC
     -100.0000    3.4609 -100.0000
    
    Colour
         2     1     2
    
    Error: Packets lost: 1, current frame num = 151 
    RangeM
        9.4454   59.2546
    
    SpeedM
       -0.0045   -0.0015
    
    Range
        9.4453   59.2500
    
    Speed
         0     0
    
    TTC
      -100  -100
    
    Colour
         2     2
    
    Error: Packets lost: 1, current frame num = 153 
    RangeM
        9.4419   55.2726
    
    SpeedM
       -0.0018  -16.1266
    
    Range
        9.4375   55.2656
    
    Speed
             0  -16.1250
    
    TTC
     -100.0000    3.4219
    
    Colour
         2     1
    
    Error: Packets lost: 1, current frame num = 155 
    RangeM
        9.4393   54.7896
    
    SpeedM
       -0.0050  -16.0767
    
    Range
        9.4375   54.7891
    
    Speed
             0  -16.0703
    
    TTC
     -100.0000    3.4063
    
    Colour
         2     1
    
    Error: Packets lost: 1, current frame num = 157 
    RangeM
        9.4148
    
    SpeedM
       -0.0041
    
    Range
        9.4141
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 159 
    RangeM
        9.4000
    
    SpeedM
       -0.0012
    
    Range
        9.3984
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 161 
    RangeM
        9.3845
    
    SpeedM
       -0.0059
    
    Range
        9.3828
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 163 
    RangeM
        9.3767
    
    SpeedM
       -0.0059
    
    Range
        9.3750
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 165 
    RangeM
        9.3681
    
    SpeedM
       -0.0057
    
    Range
        9.3672
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 167 
    RangeM
        9.3673
    
    SpeedM
       -0.0063
    
    Range
        9.3672
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 169 
    RangeM
        9.3580
    
    SpeedM
       -0.0068
    
    Range
        9.3516
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 171 
    RangeM
        9.3573    6.4880
    
    SpeedM
       -0.0066  -16.1550
    
    Range
        9.3516    6.4844
    
    Speed
             0  -16.1484
    
    TTC
     -100.0000    0.3984
    
    Colour
         2     1
    
    Error: Packets lost: 1, current frame num = 173 
    RangeM
        9.3557    6.0034   56.8173
    
    SpeedM
        0.0001  -16.1087  -16.1151
    
    Range
        9.3516    6.0000   56.8125
    
    Speed
             0  -16.1016  -16.1094
    
    TTC
     -100.0000    0.3672    3.5234
    
    Colour
         2     1     1
    
    Error: Packets lost: 1, current frame num = 175 
    RangeM
        9.3557   56.3332
    
    SpeedM
       -0.0070  -16.0304
    
    Range
        9.3516   56.3281
    
    Speed
             0  -16.0234
    
    TTC
     -100.0000    3.5078
    
    Colour
         2     1
    
    Error: Packets lost: 1, current frame num = 177 
    RangeM
        9.4000    5.4855
    
    SpeedM
       -0.0025  -16.1211
    
    Range
        9.3984    5.4844
    
    Speed
             0  -16.1172
    
    TTC
     -100.0000    0.3359
    
    Colour
         2     1
    
    Error: Packets lost: 1, current frame num = 179 
    RangeM
        9.4078    5.0063
    
    SpeedM
       -0.0001  -16.0752
    
    Range
        9.4063    5.0000
    
    Speed
             0  -16.0703
    
    TTC
     -100.0000    0.3047
    
    Colour
         2     1
    
    Error: Packets lost: 1, current frame num = 181 
    RangeM
        9.4241
    
    SpeedM
      6.0246e-04
    
    Range
        9.4219
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 183 
    RangeM
        9.4319
    
    SpeedM
       -0.0056
    
    Range
        9.4297
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 185 
    RangeM
        9.4405
    
    SpeedM
       -0.0048
    
    Range
        9.4375
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 187 
    RangeM
        9.4879
    
    SpeedM
       -0.0040
    
    Range
        9.4844
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 189 
    RangeM
        9.4957
    
    SpeedM
       -0.0032
    
    Range
        9.4922
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 191 
    RangeM
        9.5369
    
    SpeedM
      8.1967e-04
    
    Range
        9.5313
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 193 
    RangeM
        9.5688
    
    SpeedM
        0.0025
    
    Range
        9.5625
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 195 
    RangeM
        9.6085   59.2470   56.8806    7.4543
    
    SpeedM
        0.0041    0.0017  -16.1162  -16.1576
    
    Range
        9.6016   59.2422   56.8750    7.4531
    
    Speed
             0         0  -16.1094  -16.1563
    
    TTC
     -100.0000 -100.0000    3.5234    0.4609
    
    Colour
         2     2     1     1
    
    Error: Packets lost: 1, current frame num = 197 
    RangeM
        9.6404   59.2476   56.4003    6.9713
    
    SpeedM
        0.0050    0.0018  -16.1149  -16.1517
    
    Range
        9.6328   59.2422   56.3984    6.9688
    
    Speed
             0         0  -16.1094  -16.1484
    
    TTC
     -100.0000 -100.0000    3.5000    0.4297
    
    Colour
         2     2     1     1
    
    Error: Packets lost: 1, current frame num = 199 
    RangeM
        9.6715
    
    SpeedM
        0.0033
    
    Range
        9.6641
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 201 
    RangeM
        9.7042   59.2495   55.7549
    
    SpeedM
        0.0050    0.0016  -16.1402
    
    Range
        9.7031   59.2422   55.7500
    
    Speed
             0         0  -16.1328
    
    TTC
     -100.0000 -100.0000    3.4531
    
    Colour
         2     2     1
    
    Error: Packets lost: 1, current frame num = 203 
    RangeM
        9.7361   59.2500   55.2741
    
    SpeedM
        0.0067    0.0017  -16.1389
    
    Range
        9.7344   59.2500   55.2734
    
    Speed
             0         0  -16.1328
    
    TTC
     -100.0000 -100.0000    3.4219
    
    Colour
         2     2     1
    
    Error: Packets lost: 1, current frame num = 205 
    RangeM
        9.7689   59.2510
    
    SpeedM
        0.0085    0.0045
    
    Range
        9.7656   59.2500
    
    Speed
        0.0078         0
    
    TTC
      -100  -100
    
    Colour
         2     2
    
    Error: Packets lost: 1, current frame num = 207 
    RangeM
        9.8017   59.2516   54.6912
    
    SpeedM
        0.0034    0.0045  -16.1409
    
    Range
        9.7969   59.2500   54.6875
    
    Speed
             0         0  -16.1406
    
    TTC
     -100.0000 -100.0000    3.3828
    
    Colour
         2     2     1
    
    Error: Packets lost: 1, current frame num = 209 
    RangeM
        9.8258   59.2469   54.2103
    
    SpeedM
        0.0052    0.0047  -16.1406
    
    Range
        9.8203   59.2422   54.2031
    
    Speed
             0         0  -16.1328
    
    TTC
     -100.0000 -100.0000    3.3594
    
    Colour
         2     2     1
    
    Error: Packets lost: 1, current frame num = 211 
    RangeM
        9.8500
    
    SpeedM
        0.0053
    
    Range
        9.8438
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 213 
    RangeM
        9.8810
    
    SpeedM
        0.0035
    
    Range
        9.8750
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 215 
    RangeM
        9.9043
    
    SpeedM
        0.0095
    
    Range
        9.8984
    
    Speed
        0.0078
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 217 
    RangeM
        9.9268   59.2483    7.4363
    
    SpeedM
        0.0060   -0.0016  -16.1741
    
    Range
        9.9219   59.2422    7.4297
    
    Speed
             0         0  -16.1719
    
    TTC
     -100.0000 -100.0000    0.4531
    
    Colour
         2     2     1
    
    Error: Packets lost: 1, current frame num = 219 
    RangeM
        9.9492   59.2483    6.9496
    
    SpeedM
        0.0025   -0.0016  -16.1697
    
    Range
        9.9453   59.2422    6.9453
    
    Speed
             0         0  -16.1641
    
    TTC
     -100.0000 -100.0000    0.4219
    
    Colour
         2     2     1
    
    Error: Packets lost: 1, current frame num = 221 
    RangeM
        9.9708   56.6449
    
    SpeedM
       -0.0008  -16.1221
    
    Range
        9.9688   56.6406
    
    Speed
             0  -16.1172
    
    TTC
     -100.0000    3.5078
    
    Colour
         2     1
    
    Error: Packets lost: 1, current frame num = 223 
    RangeM
        9.9925   56.1610
    
    SpeedM
        0.0029  -16.0642
    
    Range
        9.9922   56.1563
    
    Speed
             0  -16.0625
    
    TTC
     -100.0000    3.4922
    
    Colour
         2     1
    
    Error: Packets lost: 1, current frame num = 225 
    RangeM
       10.0142
    
    SpeedM
     -2.7444e-04
    
    Range
       10.0078
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 227 
    RangeM
       10.0289   59.2475
    
    SpeedM
       -0.0026    0.0018
    
    Range
       10.0234   59.2422
    
    Speed
         0     0
    
    TTC
      -100  -100
    
    Colour
         2     2
    
    Error: Packets lost: 1, current frame num = 229 
    RangeM
       10.0522   59.2481
    
    SpeedM
       -0.0034    0.0019
    
    Range
       10.0469   59.2422
    
    Speed
         0     0
    
    TTC
      -100  -100
    
    Colour
         2     2
    
    Error: Packets lost: 1, current frame num = 231 
    RangeM
       10.0678   59.2475
    
    SpeedM
       -0.0018    0.0007
    
    Range
       10.0625   59.2422
    
    Speed
         0     0
    
    TTC
      -100  -100
    
    Colour
         2     2
    
    Error: Packets lost: 1, current frame num = 233 
    RangeM
       10.0911   59.2467
    
    SpeedM
       -0.0017    0.0036
    
    Range
       10.0859   59.2422
    
    Speed
         0     0
    
    TTC
      -100  -100
    
    Colour
         2     2
    
    Error: Packets lost: 1, current frame num = 235 
    RangeM
       10.1074   59.2479
    
    SpeedM
        0.0006    0.0038
    
    Range
       10.1016   59.2422
    
    Speed
         0     0
    
    TTC
      -100  -100
    
    Colour
         2     2
    
    Error: Packets lost: 1, current frame num = 237 
    RangeM
       10.1246   59.2486
    
    SpeedM
       -0.0032    0.0039
    
    Range
       10.1172   59.2422
    
    Speed
         0     0
    
    TTC
      -100  -100
    
    Colour
         2     2
    
    Error: Packets lost: 1, current frame num = 239 
    RangeM
       10.1426   59.2549    7.4141
    
    SpeedM
        0.0008   -0.0016  -16.1673
    
    Range
       10.1406   59.2500    7.4141
    
    Speed
             0         0  -16.1641
    
    TTC
     -100.0000 -100.0000    0.4531
    
    Colour
         2     2     1
    
    Error: Packets lost: 1, current frame num = 241 
    RangeM
       10.1573   59.2496    6.9251
    
    SpeedM
       -0.0008    0.0031  -16.1731
    
    Range
       10.1563   59.2422    6.9219
    
    Speed
             0         0  -16.1719
    
    TTC
     -100.0000 -100.0000    0.4219
    
    Colour
         2     2     1
    
    Error: Packets lost: 1, current frame num = 243 
    RangeM
       10.1720   59.2517   56.8737
    
    SpeedM
       -0.0032    0.0036  -16.1134
    
    Range
       10.1719   59.2500   56.8672
    
    Speed
             0         0  -16.1094
    
    TTC
     -100.0000 -100.0000    3.5234
    
    Colour
         2     2     1
    
    Error: Packets lost: 1, current frame num = 245 
    RangeM
       10.1876   59.2538    6.2949   56.3869
    
    SpeedM
       -0.0024    0.0042  -16.1668  -16.1059
    
    Range
       10.1875   59.2500    6.2891   56.3828
    
    Speed
             0         0  -16.1641  -16.1016
    
    TTC
     -100.0000 -100.0000    0.3828    3.5000
    
    Colour
         2     2     1     1
    
    Error: Packets lost: 1, current frame num = 247 
    RangeM
       10.2047   59.2501    5.8132
    
    SpeedM
        0.0008    0.0047  -16.1530
    
    Range
       10.2031   59.2500    5.8125
    
    Speed
             0         0  -16.1484
    
    TTC
     -100.0000 -100.0000    0.3594
    
    Colour
         2     2     1
    
    Error: Packets lost: 1, current frame num = 249 
    RangeM
       10.2219   59.2489   55.7399
    
    SpeedM
        0.0033    0.0028  -16.1479
    
    Range
       10.2188   59.2422   55.7344
    
    Speed
             0         0  -16.1406
    
    TTC
     -100.0000 -100.0000    3.4453
    
    Colour
         2     2     1
    
    Error: Packets lost: 1, current frame num = 251 
    RangeM
       10.2348   59.2503    5.2450   55.2593
    
    SpeedM
        0.0069    0.0031  -16.1615  -16.1398
    
    Range
       10.2344   59.2500    5.2422   55.2578
    
    Speed
             0         0  -16.1563  -16.1328
    
    TTC
     -100.0000 -100.0000    0.3203    3.4219
    
    Colour
         2     2     1     1
    
    Error: Packets lost: 1, current frame num = 253 
    RangeM
       10.2487   59.2530    4.7583
    
    SpeedM
        0.0057   -0.0025  -16.1546
    
    Range
       10.2422   59.2500    4.7578
    
    Speed
             0         0  -16.1484
    
    TTC
     -100.0000 -100.0000    0.2891
    
    Colour
         2     2     1
    
    Error: Packets lost: 1, current frame num = 255 
    RangeM
       10.2314   59.2501   54.6793
    
    SpeedM
       -0.0009   -0.0017  -16.1477
    
    Range
       10.2266   59.2500   54.6719
    
    Speed
             0         0  -16.1406
    
    TTC
     -100.0000 -100.0000    3.3828
    
    Colour
         2     2     1
    
    Error: Packets lost: 1, current frame num = 257 
    RangeM
       10.2063   59.2508   54.1988
    
    SpeedM
        0.0022   -0.0014  -16.1411
    
    Range
       10.2031   59.2500   54.1953
    
    Speed
             0         0  -16.1406
    
    TTC
     -100.0000 -100.0000    3.3516
    
    Colour
         2     2     1
    
    Error: Packets lost: 1, current frame num = 259 
    RangeM
       10.1822   59.2471
    
    SpeedM
       -0.0014   -0.0010
    
    Range
       10.1797   59.2422
    
    Speed
         0     0
    
    TTC
      -100  -100
    
    Colour
         2     2
    
    Error: Packets lost: 1, current frame num = 261 
    RangeM
       10.1649   59.2545
    
    SpeedM
        0.0027   -0.0001
    
    Range
       10.1641   59.2500
    
    Speed
         0     0
    
    TTC
      -100  -100
    
    Colour
         2     2
    
    Error: Packets lost: 1, current frame num = 263 
    RangeM
       10.1407   59.2509
    
    SpeedM
       1.0e-03 *
    
        0.0361    0.3914
    
    Range
       10.1406   59.2500
    
    Speed
         0     0
    
    TTC
      -100  -100
    
    Colour
         2     2
    
    Error: Packets lost: 1, current frame num = 265 
    RangeM
       10.1235   59.2510    7.1820
    
    SpeedM
        0.0043    0.0033  -16.1634
    
    Range
       10.1172   59.2500    7.1797
    
    Speed
             0         0  -16.1563
    
    TTC
     -100.0000 -100.0000    0.4375
    
    Colour
         2     2     1
    
    Error: Packets lost: 1, current frame num = 267 
    RangeM
       10.1062   59.2543    6.6955
    
    SpeedM
        0.0008    0.0044  -16.1549
    
    Range
       10.1016   59.2500    6.6953
    
    Speed
             0         0  -16.1484
    
    TTC
     -100.0000 -100.0000    0.4141
    
    Colour
         2     2     1
    
    Error: Packets lost: 1, current frame num = 269 
    RangeM
       10.0907   59.2517
    
    SpeedM
             0    0.0053
    
    Range
       10.0859   59.2500
    
    Speed
         0     0
    
    TTC
      -100  -100
    
    Colour
         2     2
    
    Error: Packets lost: 1, current frame num = 271 
    RangeM
       10.0666   59.2587    6.0777
    
    SpeedM
             0    0.0021  -16.1690
    
    Range
       10.0625   59.2578    6.0703
    
    Speed
             0         0  -16.1641
    
    TTC
     -100.0000 -100.0000    0.3750
    
    Colour
         2     2     1
    
    Error: Packets lost: 1, current frame num = 273 
    RangeM
       10.0527   59.2572    5.5913
    
    SpeedM
        0.0026    0.0034  -16.1612
    
    Range
       10.0469   59.2500    5.5859
    
    Speed
             0         0  -16.1563
    
    TTC
     -100.0000 -100.0000    0.3438
    
    Colour
         2     2     1
    
    Error: Packets lost: 1, current frame num = 275 
    RangeM
       10.0372   59.2557
    
    SpeedM
        0.0034    0.0048
    
    Range
       10.0313   59.2500
    
    Speed
         0     0
    
    TTC
      -100  -100
    
    Colour
         2     2
    
    Error: Packets lost: 1, current frame num = 277 
    RangeM
       10.0225   59.2542
    
    SpeedM
       -0.0017    0.0062
    
    Range
       10.0156   59.2500
    
    Speed
         0     0
    
    TTC
      -100  -100
    
    Colour
         2     2
    
    Error: Packets lost: 1, current frame num = 279 
    RangeM
       10.0105   59.2579
    
    SpeedM
        0.0047    0.0074
    
    Range
       10.0078   59.2578
    
    Speed
         0     0
    
    TTC
      -100  -100
    
    Colour
         2     2
    
    Error: Packets lost: 1, current frame num = 281 
    RangeM
        9.9899   59.2565
    
    SpeedM
        0.0036    0.0087
    
    Range
        9.9844   59.2500
    
    Speed
             0    0.0078
    
    TTC
      -100  -100
    
    Colour
         2     2
    
    Error: Packets lost: 1, current frame num = 283 
    RangeM
        9.9744   59.2552
    
    SpeedM
        0.0018    0.0101
    
    Range
        9.9688   59.2500
    
    Speed
             0    0.0078
    
    TTC
      -100  -100
    
    Colour
         2     2
    
    Error: Packets lost: 1, current frame num = 285 
    RangeM
        9.9986   59.2589   56.8714
    
    SpeedM
        0.0037    0.0113  -16.1142
    
    Range
        9.9922   59.2578   56.8672
    
    Speed
             0    0.0078  -16.1094
    
    TTC
     -100.0000 -100.0000    3.5234
    
    Colour
         2     2     1
    
    Error: Packets lost: 1, current frame num = 287 
    RangeM
       10.0178   56.3841
    
    SpeedM
        0.0089  -16.1134
    
    Range
       10.0156   56.3828
    
    Speed
        0.0078  -16.1094
    
    TTC
     -100.0000    3.5000
    
    Colour
         2     1
    
    Error: Packets lost: 1, current frame num = 289 
    RangeM
        9.9762   59.2492    7.3523
    
    SpeedM
        0.0030    0.0011  -16.1651
    
    Range
        9.9688   59.2422    7.3516
    
    Speed
             0         0  -16.1641
    
    TTC
     -100.0000 -100.0000    0.4531
    
    Colour
         2     2     1
    
    Error: Packets lost: 1, current frame num = 291 
    RangeM
        9.9772   59.2528   55.7411    6.8706
    
    SpeedM
        0.0031    0.0021  -16.1518  -16.1706
    
    Range
        9.9766   59.2500   55.7344    6.8672
    
    Speed
             0         0  -16.1484  -16.1641
    
    TTC
     -100.0000 -100.0000    3.4453    0.4219
    
    Colour
         2     2     1     1
    
    Error: Packets lost: 1, current frame num = 293 
    RangeM
        9.9617   55.2538
    
    SpeedM
        0.0022  -16.1509
    
    Range
        9.9609   55.2500
    
    Speed
             0  -16.1484
    
    TTC
     -100.0000    3.4141
    
    Colour
         2     1
    
    Error: Packets lost: 1, current frame num = 295 
    RangeM
        9.9471
    
    SpeedM
        0.0051
    
    Range
        9.9453
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 297 
    RangeM
        9.9335
    
    SpeedM
     -4.0568e-04
    
    Range
        9.9297
    
    Speed
         0
    
    TTC
      -100
    
    Colour
         2
    
    Error: Packets lost: 1, current frame num = 299 
    RangeM
        9.9189   59.2488
    
    SpeedM
        0.0007    0.0025
    
    Range
        9.9141   59.2422
    
    Speed
         0     0
    
    TTC
      -100  -100
    
    Colour
         2     2
    
    Error: Packets lost: 1, current frame num = 301 
    RangeM
        9.9121   59.2497
    
    SpeedM
        0.0028   -0.0042
    
    Range
        9.9063   59.2422
    
    Speed
         0     0
    
    TTC
      -100  -100
    
    Colour
         2     2
    
    Error: Packets lost: 1, current frame num = 303 
    >> 

    Regards,
    Carlo

  • Hi,

    Yes, the reason for this is that the Matlab processing is too slow.

    Customer should try to only record and not display any data to reduce Matlab processing.

    For matlab questions customer could find more help on mathworks support forum

    thank you

    Cesar