Dear team,
Could you please help recommend one device to replace ACS725LLCTR-50AB-T. I find our TMCS1101-Q1 has the same function with ACS725LLCTR-50AB-T, and they are also P2P compatible. But our max current is only 30A. The customer hopes our device can support >50A current, and their requirement is as below, could you please help recommend the appropriate device to me? Thank you!
1. power supply is 3.3V;
2. Support bidirectional current sensing, and support >50A current.
Thanks & Best Regards,
Sherry