Hi TI,
We have an industry radar application (2T4R) project installed on road roller has two issues,
1. Y=3m around has ghost detection for TX1 and TX2 both, and JPN customer using metal to stay behind the radar radome then the ghost gone.
2. Y=1m there is objects when moving backward which is not the real case
Please advise the SDK if any parameters to tweak with since it is bit older one chip that I am not sure if range/doppler/Clutter removal/CFAR ([解疑][TI]TI毫米波雷达系列(五):恒虚警算法(CFAR)原理_指甲的博客-CSDN博客)/AoA for the point clouds
Please advise if there is something antenna can root causing as we may plan to run HFSS
Thanks!
BR. Wilson