This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM95071: What does the temperature accuracy represent?

Part Number: LM95071


Hello Team,

 

The maximum temperature accuracy of LM95071 is 1, according to the datasheet.

Which does this accuracy represent absolute accuracy or repeatability?

Best regards,

Kanda

  • Hi Kanda,

    The maximum temperature error listed in the datasheet represents the accuracy of the LM95071. Please note that the maximum temperature error varies with the temperature as shown in Figure 5 of the datasheet, and therefore the accuracy is affected as well.

    Best Regards,

    Andrew Yu