Other Parts Discussed in Thread: LDC1314, TIDA-00508
Team,
Customer is using the LDC1314DIAL-EVM HW and TIDA-00508 GUI SW for evaluation.
Now they have their own LDC1314 coil and target PCBs and would like to test it with our LDC1314DIAL-EVM MCU board (see below).
Their prototype has the same connector as used in our EVM. The coil/target is not a 100% match to our EVM design as it does not support 360 deg, but only appr 300 Deg.
Overall the GUI shows precise displacment following the target movement.
However they see some glitches (ie the GUI arrows jumps from time to time).
What could cause those glitches (issues with coil/targets or SW not adapted for custom target/coils)?
Was the LDC1314DIAL-EVM intended to be used as well to test custom targets/coils?
Can we make the MCU side SW available (not the PC side) in order to debug and help them test further using our GUI?
There is a JTAG connector on the board so I assume the MCU can be reflashed and modified provided that we can share the src code.
Thanks in advance!
A.