Other Parts Discussed in Thread: AWR1843
Hareware:AWR1843 BOOST
Software:lab0007_medium_range_radar
HI,I want remove the the height measurement function of USRR30 of MRR,What parts of the code should I make changes?
because after testing, I found that the detectable FOV of usrr20 with the same target in MRR is less than that of usrr20 in SRR.
For example, for the same PVC pipe, usrr20 in SRR can see 0 5m@75 However, usrr20 in MRR can only see 0 5m@45 °,
I don't know why, I think one of the reasons may be the height measurement function in MRR, so I want to try to remove the height measurement function in MRR,
So what should i do?