Other Parts Discussed in Thread: TM4C123GH6PM, IWR6843, MMWAVEICBOOST
I am trying to use the IWR6843 board along with mmwaveBoost IC and Tiva launchpad (Part number : TM4C123GH6PM) as shown in the below snapshot.
I want to transfer the LVDS data that is received by the mmwaveICBoost from IWR6843 to TM4C123GH6PM board and do some small processing on the tiva board itself.I would like to know what is the significance of the below pins and is it possible to transfer data to tiva lauchpad.
Also Is it possible to do the processing on the LVDS/UART data given by IWR6843 on mmwaveIC Boost or IWR board it self ? I want to derive two paramters out of my experimentation which i can display on a LCD.