This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: 14xx - mmWave SDK Demo Build Error

Part Number: IWR1443


Dear TI, 

I am trying to build the 14xx - mmWave SDK Demo in CCS. I downloaded and installed the project using the Resource Explorer within CCS . I have followed the Setup Guide and ensured all the pre-requisites listed are downloaded correctly.

When I rebuild the Demo, I get the following errors:

"../main.c", line 734: error #20: identifier "MMWAVE_L3RAM_NUM_BANK" is undefined
"../main.c", line 734: error #20: identifier "MMWAVE_SHMEM_BANK_SIZE" is undefined

Other online threads seem to suggest this is due to the SDK version used. I am currently using mmWave SDK 2.1.0.04 (as recommended by the Setup Guide). I am also using CCSv8.3.1 because CCSv10.3.1 was not compatible.

Any assistance you could provide to fix these errors would be greatly appreciated.

Regards,

Mietta