This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDEP-01012: frequency calibration in Antenna Calibration

Part Number: TIDEP-01012


Please let me conform frequency calibration formula in Antenna Calibration.

N_chirp: the number of ADC samples per chirp
N_calib: the number of ADC samples per chirp at calibration
n_chirp = [0 N_chirp-1]

 
TI document:   C:\ti\mmwave_studio_03_00_00_14\mmWaveStudio\MatlabExamples\signal_processing_4chip_cascade.pdf at Page 9.
(script C:\ti\mmwave_studio_03_00_00_14\mmWaveStudio\MatlabExamples\4chip_cascade_MIMO_example\modules\calibration\@calibrationCascade\datapath.m)
F = 2*pi *P_diff * f_s^calib/f_s^chirp* f_chirp/f_calib / (N_chirp*FFTTimes) * n_chirp (1)

My opinion
F = 2*pi *P_diff * f_s^calib/f_s^chirp* f_chirp/f_calib / (N_calib*FFTTimes) * n_chirp (1)

I guess N_calib is right.

where P_diff is the FFT peak index difference for a virtual channel; f_chirp is the FMCW chirp frequency slope; f_calib is the FMCW chirp frequency slope used for calibration which can be different from f_chirp; f_s^calib is the FMCW chirp sampling rate used for calibration which can be different from the sampling rate ℎ applied in the actual data.

 

Detail

  • freq compensation at calibration: freqComp1

freqComp_calib = (FFTbinIdx1-FFTbinIdxRef)/FFTTimes/N_calib*f_s^calib

 

fRef =FFTbinIdxRef/FFTTimes/(N_calib/2)*f_s^calib/2 : ref peak

f1 =FFTbinIdx1/FFTTimes/(N_calib/2)*f_s^calib/2 :turned peak

freqComp_calib =f1-fRef

 

  • target freq compenstion : freqComp_chirp

timeComp_calib=freqComp_calib/f_calib

timeComp_chirp=freqComp_chirp/f_chirp

if timeComp_calib = timeComp_chirp

 

freqComp_chirp=timeComp_chirp*f_chirp

freqComp_chirp= freqComp_calib/f_calib *f_chirp

 

  • How to apply freqComp to ADCData_chirp

ADCData_chirp.*exp(1j*2*pi-freqComp_chirp*n_chirp*1/f_s^chirp)