This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP461-SP: Termination of remote sense pins on the IC

Part Number: TMP461-SP

Hi,

So the customer wants to use TMP461-SP device for only local sensing purpose. He does not require it for remote sensing. So how does he terminate the D+ and D- pins? No guideline is given in the datasheet for the same.

Thanks & Regards,

Jash Kothari

FAE

  • Hi Jash,

    If remote sensing is not required, D+ must be connected to D- or GND in order to prevent unnecessary fault warnings. Please refer to section 7.3.5 or section 8.1 of the datasheet for further information on this.

    Best regards,

    Nicole