Other Parts Discussed in Thread: MMWCAS-DSP-EVM, MMWCAS-RF-EVM
Hello!
I has MMWCAS-RF-EVM board with MMWCAS-DSP-EVM module. I already try to use GUI mmWaveStudio tools for Cascade radar mode, now i try to run example from
"mmwave_dfp_02_02_00_03\ti\example\mmWaveLink_Cascade_Example" and PC can't connect to TDA board via ethernet. The log from console is:
INFO: Registered Async event handler with TDA
Device map 32 : CAPTURE_RESPONSE_ACK Async event recieved with status 0
ERROR: Connecting to TDA failed with error 1. Check whether the capture card is connected to the network!
ERROR: Failed to Connect with TDA
I Already ping the board, and try to connect via GUI it's work fine, but in this example connection don't work.