This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: AWR1843

Part Number: AWR1843

Working on a board using AWR1843. Just wonder if we could program the frequency to 75 GHz or lower.

Thanks,

Henry

  • Hello Henry, 

    The wide range of TI highly integrated 77GHz and 60GHz CMOS TI mmWave sensors are tabulated in the table below : 

    These are the ONLY frequency supported. Corresponding to AWR1843, you can see the expected frequency operating region is 76-81GHz (as mentioned in the device datasheet as well). 

    Regards,

    Ishita