This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: profileCfg issue

Part Number: IWR6843AOP

hi,

I was trying to configure a shorter distance profile in over head people counting based on a working profileCfg command:
profileCfg 0 61.2 60.0 17.0 50.0 328965.0 0.0 99.27 1.0 64 1000 2.0 1.0 36

According to my understanding, the distance is related with the tx power and sampling rate. I kept the tx power untouched and set the digOutputSampleRate to 1000 (a half), then got an error message -1 from sensor.

I also tried to combine lower digOutputSampleRate with shorter ramp end time and failed without luck.

Would you guys please point out what parameters else I should modify in order to sensor shorter distance? The target range is 3m.

thinks.

  • Hi, 

    Have you already looked at the user guide

    https://www.ti.com/lit/an/swra553a/swra553a.pdf

    This should help the customers design their own chirp profile. Please let me know if this user guide did not help resolve the issue mentioned above. 

    Regards, 

    Sudharshan K N 

  • Hi, Yes, I have read the doc you referred for a couple of times and understand how to design chirps. But still not able to figure this out. Would you experts give some hints on this?

  • Hi, 

    Can you please let me know which sample configuration are you looking at? Is this from the SDK 3.5 labs? 

    Regards, 

    Sudharshan K N 

  • Hi,

    here is the cfg from the overhead people counting (470) project:

    sensorStop
    flushCfg
    dfeDataOutputMode 1
    channelCfg 15 7 0
    adcCfg 2 1
    adcbufCfg -1 0 1 1 1
    lowPower 0 0
    profileCfg 0 61.2 60.00 17.00 50 328965 0 55.27 1 64 2000.00 2 1 36
    chirpCfg 0 0 0 0 0 0 0 1
    chirpCfg 1 1 0 0 0 0 0 2
    chirpCfg 2 2 0 0 0 0 0 4
    frameCfg 0 2 224 0 120.00 1 0
    dynamicRACfarCfg -1 10 1 1 1 8 8 6 4 4.00 6.00 0.50 1 1
    staticRACfarCfg -1 4 4 2 2 8 16 4 6 6.00 13.00 0.50 0 0
    dynamicRangeAngleCfg -1 7.000 0.0010 2 0
    dynamic2DAngleCfg -1 5 1 1 1.00 15.00 2
    staticRangeAngleCfg -1 0 1 1
    %classifierCfg 1 1 1 500 0.6 1.0 0.95 10
    antGeometry0 -1 -1 0 0 -3 -3 -2 -2 -1 -1 0 0
    antGeometry1 -1 0 -1 0 -3 -2 -3 -2 -3 -2 -3 -2
    antPhaseRot -1 1 -1 1 -1 1 -1 1 -1 1 -1 1
    fovCfg -1 64.0 64.0
    compRangeBiasAndRxChanPhase 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 
    staticBoundaryBox -3 3 -3 3 -0.5 3
    boundaryBox -4 4 -4 4 -0.5 3
    sensorPosition 2.9 0 90
    gatingParam 3 2 2 3 4
    stateParam 3 3 6 20 3 1000
    allocationParam 20 20 0.05 20 1.5 20
    maxAcceleration 1 0.1 1
    trackingCfg 1 4 800 20 37 33 120 1
    presenceBoundaryBox -4 4 -4 4 0.5 2.5
    sensorStart

    thanks.
  • Hi, 

    Sorry for the late response. 

    The detection range can also be reduced by changing the boundary box parameters. Let me know if this served the purpose. 

    Regards, 

    Sudharshan K N