This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: Solution for connecting 4x AWR2243 to TDA4VM

Part Number: AWR2243
Other Parts Discussed in Thread: TDA4VM

Hi TI experts,

Is there a solution for connecting 4x AWR2243, which results in 4 CSI-2 modules each with 4 lanes, into a TDA4VM, which has only 2x CSI-2 modules ?

I think one possible option is to use TI FDP-Link Serializer and Deserializer. However I think this option is used when one has to connect the AWRs and TDA4VM locating far away from each other over a STP/Coax cable. When both AWRs and TDA4VM are located on the same PCB, this option does not seem to be the best option and also relatively expensive.

So my question is:

    - Is there a more cost effective and better suited solution for interfacing 4x AWR2243 to TDA4vm when they are located on the same PCB or close to each other ?

Thanks

BL