This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: angle estimation

Part Number: IWR6843AOPEVM


Greetings,

i have a question regarding the angle estimation technique that the IWR6843AOPEVM is using. Are Azimuth and Elevation only calculated by measuring the phase difference between the received signals for every frame, so that only one transmitter at the time is active? Or are the transmitters all active at once to generate some kind of beamforming like it is the case with phased array antennas?

Regarding to the "fundamentals" document it should be the angle or arrival method, right? What is the purpose of multiple transmitters then if they are only used one after another?

Regards, 

Jens Bühler