We are planning to develop a proximity sensor that utilizes the LDC0851.
First, we are considering introducing an evaluation module (LDC0851EVM) to see if the LDC0851 can perform the desired proximity sensing operation.
Please let me know the following.
1. How to connect the LDC0851EVM to a sensor (coil) that the user can easily use
What restrictions are there on removing the sensor part of the LDC0851EVM and connecting it to the coil in our product system?
I have read the manual for the LDC0851EVM, but it only describes the coil inside the EVM.
I have read the manual for the LDC0851EVM, but it only describes the coil inside the EVM, so I would like to check if it is possible to connect the user coil (the part I want to use as a sensor).
I would like to confirm if it is possible to connect to a user coil (the part I want to use as a sensor).
We would like to use our product coil itself as a proximity sensor to check contact with the end user's mold without using a commercially available proximity sensor.
We would like to use our product coil itself as a proximity sensor to confirm contact with the end user's mold without using a commercially available proximity sensor.
Composition
End-user's metal mold ★Sensor (product coil)--LDC0851EMV evaluation module
Controller
2. Setting the conditions for using the user coil as a sensor
Please provide us with the manual that we should refer to in order to conduct the operation experiment described in section 1.
Above.