Hi Team,
We have received this inquiry from our customer,
I am currently developing a radar with sports applications, but we require high accuracy and, as such, need to move towards mmwave radar solutions
However, I am wondering if I can use the automotive radar solutions in this application as well?
If not, which alternative do you recommend?
To be more specific: I would like to use this evaluation kit to build a test setup www.ti.com/.../MMWCAS-RF-EVM
The radar would be used to track a golf ball
So we need to determine several golf parameters, during the swing and launch
(not so much flight, as this won't be feasible with standard mmwave radar)
So we need a high angular resolution, a high spatial resolution and velocity resolution
That's why I would like to use a 60 GHz or 80 GHz radar (with 4GHz or more bandwidth), as the 24 GHz radars only provide 250 MHz bandwidth
Also, the ability to cascade multiple radar chips to enable very high angular resolution in a MIMO configuration seems very attractive for our application as well
But this functionality is only provided in the automotive mmwave sensors (www.ti.com/.../MMWCAS-RF-EVM)
No, you can see it more as a golf simulator tool. We determine the parameters during launch (with high accuracy) to simulate the rest of the flight.
Does our automotive mmWave sensors suitable for this application?
Regards,
Danilo