Hello,
There is the below note on page 7 of the datasheet(SNAS648B).
(4) PT1000 RTD approximate resistance: 800 Ω ≡ –52°C, 931 Ω ≡ –18°C, 1.10 kΩ ≡ 26°C, 1.33 kΩ ≡ 86°C and 1.48 kΩ ≡ 125°C.
Does it mean maximum RTD resistance value that TDC1000 can measure accurately value is 1.48Kohm?
If measuring over 1.48Kohm, is it still accurate?
My customer is considering to put a series resistor to PT1000 line for ESD protection.
Regards,
Oba