This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: AWR2243 vs AWR1843 vs AWR1642 maximum distance ?

Part Number: AWR2243
Other Parts Discussed in Thread: AWR1843, AWR1642

Hello Guys,

Good day.

Our customer is mainly interested on application for the maximum possible distance. He saw that the AWR2243 provides a IF bandwidth of 20 Mhz while the AWR1843 provides the half (10 MHz) IF bandwidth.

Does this translate into the double maximum distance?
He have checked the document "object vs range" (www.ti.com/.../swra593a.pdf) but it looks that it is for the family of the 1642 with a bandwidth of 5 MHz.

He knows the problem of not having DSP and hardware accelerator included in the AWR2243 but he wanted to know if this double IF bandwidth is (approximately) translate into a double performance in the maximum distance.

Is there a new document with the performance for the new devices? Which improvement in the performance can they expect with the increase of IF bandwidth to 10 MHz and 20 MHz? They just want rough number. They know that it is not something exact and will depend on many factors.

Thanks and regards,

Art