Other Parts Discussed in Thread: IWR6843, AM3358
Hi,
Please find attached design query list.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Please find attached design query list.
Hi Akash,
Design query for IWR6843AOP,
Sr no | Section | Interface | Query |
1 | IWR6843AOP | PMIC | Ferrite bead used in EVM for PMIC section are not as suggested by Datasheet, which one to use? |
2 | IWR6843AOP | PMIC | Datasheet suggested 100nF for VANA de-cap, but in EVM design 220nF is used. Which one to follow, EVM schematic or datasheet ? |
3 | IWR6843AOP | PMIC | PMIC_CLKOUT from IWR6843 is not used for PMIC IC, as per datasheet it can help in decrease voltage noise. Do we need to use it? |
4 | IWR6843AOP | PMIC | Any advantage of using PMIC over regular DCDC? PMIC looks more expensive than DCDC. |
5 | IWR6843AOP | nReset | How much delay should be provided between SOP and RESET enable? |
6 | IWR6843AOP | Clock | Do we need SYNC IN and SYNC OUT signal when using stand alone, without booster board ? |
7 | IWR6843AOP | OSC_CLKOUT | Do we need to have OSC_CLKOUT test point or SMA connector? What parameter we can measure on OSC_CLKOUT? |
Thanks,
Yash
Hi Yash
For the first one the first question the PMIC LP87524 is specified in the datasheet for the J and P variants. It can be found in the datasheet here.
For the other questions I will need more time and will need to loop in a hardware expert. Please allow several days for a response.
Regards,
AG
Hello Yash,
1. For the secondary LC filter (after the PMIC LC filter), you should use the blm18kg121th1d ferrite. Which part number are you referring to specifically?
2. Use the same decaps as in the EVM
3. PMIC_CLKOUT is not required. By default this pin will not be configured as a clock unless you enable it in the pinmux.
4. The radar is very sensitive to supply noise. We recommend to only use designs that have been validated and tested on our EVM. Using other supplies could result in poor RF performance depending on the noise specifications of the supply.
5. There is no fixed delay. As long as all supplies are stable and the SOP pins are stable, NRST can be released. The timing of this will depend on how you are driving the SOP pins and how you are driving the supplies.
6. No, SYNC_IN and SYNC_OUT are not required. These are only needed if you want to trigger the frame from an external source.
7. For your first board design, we recommend to bring out OSC_CLK. This can be used to help tune the XTAL frequency in case you need to adjust the load caps on the XTAL.
Regards,
Adrian
Hi,
Please find attached Schematic for review. We are using mmWave IC IWR6843 with AM3358 SoC.
Hello Yash,
We can't do a full schematic review on E2E. If you would like a general schematic review, please get in contact with your local field sales office.
If you have any specific questions that are not related to this thread, please start a new thread. If the questions you had in this thread were not addressed, please let us know what further clarifications are needed.
Regards,
Adrian