This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC2114EVM: A problem about setting the register of drive current

Part Number: FDC2114EVM


I'm testing the FDC2114EVM using the EVM GUI. When i set the register of the drive current, I found the frequency changes with the drive current. This is normal? Where is my issue?

I used the singal channel,and control the Vpk between 1.2 to 1.6V. And the settle count and reference count are set with the values from the datasheet because my cap is similar as the example.