This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: why the power of a chirp between a frame is different?

Part Number: IWR1843BOOST
Other Parts Discussed in Thread: DCA1000EVM,

Hi, I use IWR1843BOOST and DCA1000EVM detecting a wall far from the radar about 4 meters.

I add the absolute value of all the adc samples of a chirp, and then I get the following result

this is 5000+ points, every point represent the sum of all the adc samples' absolute value of a chirp. the following picture is 3 frames, and these is 64 chirps in a frame.

I want to know why the power of  per chirp in a frame is different, and it seems has a kind of Periodicity.