Hello,
I am using the IWR6843ISK Board with Default Firmware.
When I set 'Antenna Config=4Rx,3Tx' in mmWave Demo Visualizer, I get 'numTlv=4' in the binary record file (.dat).
However, the sample script in SDK (../mmwave_sdk_03_05_00_04/packages/ti/demo/parser_scripts/parser_mmw_demo.py) is only described the processing of 1st TLV (Type=1) and 2nd TLV (Type=7).
Is there a document that contains the data specifications of remaining two TLVs ? (Type=2, 512bytes & Type=3, 512bytes)
Regards,
Tomo