This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP411: not using remote sensor

Part Number: TMP411


Hi Team,

My customer is not using the remote sensor function, so they follow the DS description to short the D+ and D- together as below.

There is a question about the Pin6 behavior. Before any configuration or setting. The customer measured on the pin 6 alert#, the output was 0V LOW. (which shall means triggered)
Please advise if this is the behavior of the sensor by default before changing any setting? Thank you.

And the customer also measured the pin 4 Therm#, the output was 3.3V high.

Best regards,

Mike