This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC7201: How to restart a new measurement before stop signal input?

Part Number: TDC7201

Hello guys,

One of my customers is evaluating TDC7201 for their new products.

At this moment, they have the following questions about TDC7201.

Could you please give me your reply?

Q.  TDC7201 datasheet (version:SNAS686) says that a new measurement is started when the START_MEAS bit in the TDCx_CONFIG1 register is changed from "0" to "1".

      After that, the measurement is finished when STOP signal is input.

      But they think there are cases where they want to restart a new measurement even though STOP does not come as a condition.

.     For this restart, are the following sequence ((1)~(3)) correct?

      (1) Write "1" to NEW_MEAS_INT bit in TDCx_INT_STATUS register.

      (2) START_MEAS bit in the TDCx_CONFIG1 register is set to "0" by action (1) .

      (3) Write "1" to START_MEAS bit in the TDCx_CONFIG1 register.

Your reply would be much appreciated.

Best regards,

Kazuya.

  • Hello Kazuya,

    Thank you for your question. That is the correct sequence of events to conduct a new measurement without using a stop signal. 



    Please let me know if you have any other questions regarding the TDC7201.

    Thank you,

    Jacob