Other Parts Discussed in Thread: TMAG5273, , TMAG5170
Hi Team,
Can you comment on the following questions regarding TMAG5170-Q1 as well as TMAG5273?
- Sensitivity error: Is this error always of the same amount (systematic error) when the exact same chip is used for multiple measurements and is only varying from chip to chip? This would mean it can be calibrated out by the customer
- Software: Are there C drivers available for each device?
- Measurement: How many bits are being pushed out of the interface with each measurement?
- Version: When will version A1 of TMAG5273 be available?
Thank you,
Franz