This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: CSI Deskew calibration function

Expert 7150 points
Part Number: AWR2243


Hi Experts,

My customer is building their own cascade board with AWR2243 and their back-end chip. They have some questions about CSI calibration.

1) Does AWR2243 (CSI Tx) have Deskew calibration function? (i.e. Should their back-end chip (CSI Rx) support Deskew calibration function?)
2) If (1) is yes, when does the function work? For instance, in initialization phase, periodically, etc)
3) If (1) is yes, Is it possible to execute it manually by issuing AWR command/API?

Best regards,
Ken