Hi,
I have couple questions about AFE3010.
1. In the datasheet, it says "Supports 120-V/ 60-Hz or 220-V/ 50-Hz systems." Does that mean AFE3010 could support to the range of 120V to 220V AC input and with the range of 50hz to 60hz? For example, AFE3010 does not just support 120V/60hz, it also supports 120V/50hz.
2. If we want to wire the alarm bit to the host MCU which is in the secondary side, should we add optocoupler so that alarm bit is connected to the GND of secondary side?
Thanks.