Other Parts Discussed in Thread: AWR1843AOP, AWR1843BOOST, AWR1843
Hi,
I have recently bought the AWR1843AOPEVM, i was able to run the demo with the mmwave demo visualizer and make some tests with the targets in an open field. The radar looks fine and it is working as expected. However i have some questions:
First question:
I want to work with the radar with different configurations, i see that here C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/xwr18xx/mmw/docs/doxygen/html/index.html there is information about the demo but i was not able to find a document where i can see which parameters from the radar i can set up. More in detail, i would like to know how to change the different frame parameters to have the best range or range resolution ( i see that there is an option in the visualizer but i want to have the full control trough the messages sent it trough the port). The Messages like:
mmwDemo:/>adcbufCfg -1 0 1 1 1
Done
mmwDemo:/>profileCfg 0 77 267 7 57.14 0 0 70 1 256 5209 0 0 30
Done
I see there is some examples here C:\ti\mmwave_sdk_03_05_00_04\packages\ti\demo\xwr18xx\mmw\profiles and the mmWave Demo Visualizer pdf document SWRU529C but there is no a proper explanation of each of the numbers.
I was able to send these CLI commands using python through corresponding COM port but i still do not understand some of them.
Second question
A second question is related to the tx power, i see in the datasheet that the power is 16 dbm, is this the maximum power? is this fixed or can be changed in the configuration? When i use the demo, is the radar using this 16 dbm?
As for my application i want to detect small objects, has it sense to use an external amplifier with the AWR1843AOPEVM? Should i need then to get the raw data to be able to use an amplifier?
Third question
I want to know the main differences respect to the AWR1843BOOST (which uses the AWR1843 instead of the AWR1843AOP). From the datasheets i see it looks like the only difference is the Txpower of the chip and the RX noise figure. Are there more differences?
For my application i need to detect objects in movement (i do not care about their velocity but at least to detect them) and i read in this link (https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/993522/ti-s-awr1843aop-now-available) that the AWR1843AOPEVM is "optimzed for static targets". This means that is not good to detect moving objects? should i go for the AWR1843BOOST or the performance will be similar?
Many thanks in advance,
Regards,
Victor